Machine Elements |New Product
New Products introduced : Low Profile Swivel Mounts for Control Panels, Pillar/Hanging Type
Aug. 25. 2026
Special Screws |New Product
New Products introduced : Vented Flanged Socket Head Cap Screws - Silver Plating
Jun. 30. 2026
Factory Equipment Components |New Product
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
Couplings |New Product
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
Ball joint・Angle Hinge
Structure Components
Hexagonpost
Set Collars
Indicators
Scales
Dial
Stages
Ball Rollers (Ball Transfers)
Display Mounting Systems
Swivel Mount
Auto-Positioning Units
Remote Gauge Inspection Cameras
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
SEMI Standard (SEMI S8-0218)Compliant Products
All Stainless Steel Products
All Metal Products
Universal Design Products
Jul. 06. 2026
Mar. 22. 2024
Aug. 03. 2020
Jul. 08. 2016
Aug. 19. 2014
Jul. 25. 2014
Jan. 30. 2025
Jan. 27. 2025
Nov. 07. 2023
Jun. 15. 2026
May. 14. 2026
Apr. 27. 2026
Apr. 23. 2026
Nov. 26. 2025
Jun. 28. 2024
Jan. 29. 2024
Jan. 19. 2024
Sep. 05. 2025
Oct. 25. 2016
Sep. 23. 2016
Jan. 06. 2015
Oct. 29. 2025
Dec. 02. 2024
Oct. 07. 2024
Mar. 26. 2024
Nov. 12. 2025
Nov. 10. 2025
Nov. 18. 2024
Jun. 24. 2025
Jan. 14. 2025
Feb. 17. 2025
Nov. 25. 2025
May. 16. 2025
May. 15. 2025
Jan. 10. 2025
May. 12. 2025
Apr. 30. 2025
Nov. 28. 2024
Nov. 06. 2024
Feb. 25. 2026
Dec. 22. 2025
Dec. 16. 2024
Nov. 27. 2024
Nov. 01. 2024
Description of Plungers for EngineersDescription of Machine elements for Designers Plungers Edition page. Plungers are machine elements for positioning and fixing workpieces. We offer a clear introduction to plungers, the advantages of their use, various usage examples, and their types and characteristics.Apr. 30. 2025 time >
Description of Machine elements for Designers Plungers Edition page. Plungers are machine elements for positioning and fixing workpieces. We offer a clear introduction to plungers, the advantages of their use, various usage examples, and their types and characteristics.
Apr. 30. 2025 time >
CE-marked components which prevent foreign matter contamination are required 【Safety / precautionary measures】Introducing components with a captive mechanism.Mar. 25. 2025 time >
Introducing components with a captive mechanism.
Mar. 25. 2025 time >
Products conforming to SEMI standards are required【Safety Measures/Precautionary Measures】Introducing our abundant lineup of SEMI standard compliant products.Mar. 12. 2025 time >
Introducing our abundant lineup of SEMI standard compliant products.
Mar. 12. 2025 time >
About SUH660SUH660 is austenitic heat-resistant steel. With high strength at high temperatures, it can be used in environments up to 700°C.Jan. 28. 2025 time >
SUH660 is austenitic heat-resistant steel. With high strength at high temperatures, it can be used in environments up to 700°C.
Jan. 28. 2025 time >
General TolerancesThis page describes JIS B 0405 / JIS B 0419 "General tolerances".Jan. 27. 2025 time >
This page describes JIS B 0405 / JIS B 0419 "General tolerances".
Jan. 27. 2025 time >
Hexagon NutsThis page describes JIS B 1181 "Hexagon Nuts (those not dependent on ISO 4032 to 4036 and ISO 8673 to 8675)".Jan. 27. 2025 time >
This page describes JIS B 1181 "Hexagon Nuts (those not dependent on ISO 4032 to 4036 and ISO 8673 to 8675)".
Key and Their Corresponding KeywaysThis page describes JIS B 1301 "Keys and their corresponding keyways".Jan. 27. 2025 time >
This page describes JIS B 1301 "Keys and their corresponding keyways".
Dimensions of Holes for Hexagon Socket Cap ScrewsThis page describes "Dimensions of Holes for Hexagon Socket Cap Screws".Jan. 27. 2025 time >
This page describes "Dimensions of Holes for Hexagon Socket Cap Screws".
What makes our custom screws specialThe machine parts manufacturer Nabeya Bi-tech Kaisha (NBK) at e-nedzi.com manufactures special screws to the customer's specifications, such as tip machining and surface treatment. Special material screws, resin screws and loosening prevention are also available.Jan. 14. 2025 time >
The machine parts manufacturer Nabeya Bi-tech Kaisha (NBK) at e-nedzi.com manufactures special screws to the customer's specifications, such as tip machining and surface treatment. Special material screws, resin screws and loosening prevention are also available.
Jan. 14. 2025 time >
Vol. 13 Explaining the Rust Source "Galvanic Corrosion"Have you ever been surprised by rust suddenly appearing on rust-resistant aluminum? If this happens, the reduced strength resulting from the corrosion brings fears of possible damage. This phenomenon is known as "galvanic corrosion". Today, I will explain this principle and how it can be handled. Jan. 10. 2025 time >
Have you ever been surprised by rust suddenly appearing on rust-resistant aluminum? If this happens, the reduced strength resulting from the corrosion brings fears of possible damage. This phenomenon is known as "galvanic corrosion". Today, I will explain this principle and how it can be handled.
Jan. 10. 2025 time >
What is a Linear Guide Stopper? Introduction to Types and Features!It is a component used to prevent slip-out, falling, and to act as a stopper in case of uncontrolled movement for linear guideways (linear ways, linear guides, slide rails). Nov. 28. 2024 time >
It is a component used to prevent slip-out, falling, and to act as a stopper in case of uncontrolled movement for linear guideways (linear ways, linear guides, slide rails).
Nov. 28. 2024 time >
Vol.6 Varieties of Screws "Beyond" SUSProbably most of the screws you use are made of either iron or stainless steel. However, there are also screws made from various other materials that possess very interesting characteristics. Perhaps these may be able to resolve some of your problems that you have encountered with iron and stainless steel screws. Today, Nedzigon is here to introduce you to the different types and features of screws made of special materials. Nov. 18. 2024 time >
Probably most of the screws you use are made of either iron or stainless steel. However, there are also screws made from various other materials that possess very interesting characteristics. Perhaps these may be able to resolve some of your problems that you have encountered with iron and stainless steel screws. Today, Nedzigon is here to introduce you to the different types and features of screws made of special materials.
Nov. 18. 2024 time >
What are clamp levers? Here we explain the characteristics and usage methods that help streamline screw tightening!Description of Machine elements for Designers Clamp Levers Edition page. We introduce here what clamp levers are, the advantages of their use, various usage examples, and their types and characteristics.Nov. 06. 2024 time >
Description of Machine elements for Designers Clamp Levers Edition page. We introduce here what clamp levers are, the advantages of their use, various usage examples, and their types and characteristics.
Nov. 06. 2024 time >
Chemical Resistance of Chemical-proof ScrewsThis page describes "Chemical Resistance of Chemical-proof Screws" such as ceramic, titanium, resin nickel and Inconel.Oct. 07. 2024 time >
This page describes "Chemical Resistance of Chemical-proof Screws" such as ceramic, titanium, resin nickel and Inconel.
Oct. 07. 2024 time >
Property of Special Material ScrewsThis page describes "Properties of Special Material Screws" such as ceramic, nickel, aluminum, molybdenum, Inconel, Hastelloy and phosphor bronze.Oct. 07. 2024 time >
This page describes "Properties of Special Material Screws" such as ceramic, nickel, aluminum, molybdenum, Inconel, Hastelloy and phosphor bronze.
Screws must be protected from chemicals 【Energy-saving / reduced work-hours】Introducing screws with excellent chemical resistance and screws with head coatings.Oct. 07. 2024 time >
Introducing screws with excellent chemical resistance and screws with head coatings.
NEW SAVE