Date Published:Dec. 02. 2024

Preventing gaps between the sheet and screw when fastening thin sheets

Use screws suitable for fixing thin plates

With common screws that have incomplete threads, a gap may occur because the screws cannot be fully tightened when fixing thin plates.
By using screws designed for fixing thin plates with relief machining under the head, it is possible to fix thin plates without any gaps.

sukima-en

Recommended Products

Hexagon Soket Ultra Low Head Bolts for Thin Plate Fastening
SSHS-UC

➡View All Sheet Metal Fasteners

Issue/case studies Improved productivity/workability Reduced cost/energy saving/long life Solution samples Special Screws