NBK logo

Date Published:Sep. 06. 2024

Quickly checking the status of machines and equipment visually

There are LED-equipped handles that allow you to check the status of machines and equipment at hand.

By installing the LED illumination linked to the equipment in the worker's line of sight...

▶You can check the status of the equipment at hand without having to look up at the signal tower.
 Additionally, having the LED in the worker's path is also effective in preventing overlooking the signal tower.

▶By equipping the handle with this function, you can prevent working while the interlock is accidentally released.
 The type with a switch allows you to send an electric signal with switch operation, enabling the locking and unlocking of the interlock.(Interlock equipment is required separately.)

Recommended Products

Plastic Handles with LED

Issue/case studies Safety measures/precautionary measures Solution samples Machine Elements