Date Published:May. 14. 2020

Shaft radial load must be suppressed 【Automation / robots / motorization】

Couplings with constant speed and excellent low-eccentric reaction force should be used

Bar feeder encoder

Miniaturization of the encoder and sensor means that the radial load applied to the shaft increases to the extent of straining the shaft, making suppression of shaft radial load an issue. Bellows couplings can tolerate radial loads and rotate at constant speed even if load on the shaft causes misalignment. Their low eccentric reaction force allows use without impairing encoder and sensor performance.


Recommended product

Bellows Couplings  MFB-C

Issue/case studies Automation/robots/motorization Machine Tools Semiconductor Manufacturing Equipment Food Machinery Automotive Manufacturing Process Medical Equipment FA Devices Solution samples Couplings